This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

1.8V input, 0.8V output, 300 mA 、 PSRR greater than 70 dB @1kHz 、SOT23-5 package



Dears,

Can you show me the IC that the replacement type of pin to pin with RT9078N-08GJ5;

1) 1.8V input, 0.8V output, 300 mA
2) PSRR greater than 70 dB @1kHz
3) SOT23-5 package,

Thank you .