Part Number: UC2843
What are the ramifications of allowing a continuous conduction fixed frequency flyback power supply go from Continuous to Discontinuous operation?
I've inherited a design where the load on the CCM fixed frequency power supply was significantly overestimated. As a result the flyback is crossing into DCM operation under actual low load conditions. Tehere really isn't adequate time to go back to the drawing board to redesign the circuit. Is this actually Bad?
All the information I've found seems to assume a supply is designed to be either CCM or DCM. What issues do I need to look with a supply operating in both modes? Could there be serious issues that hide right at the threshold between the two operating modes?