Other Parts Discussed in Thread: CSD16404Q5A
Hi,
BQ24600 IC is been used in the charging circuit for one of our application.
I've been facing an issue of battery charging!! The pack is not getting charged!
The circuit is designed for 4 cells in parallel lithium-ion pack with charge current of 4A.
The circuit is exactly same as the EVM with change of the part for MOSFETs (instead of SiR4260p, Im using CSD16404q5a),
The voltages at VIN=12, Vref=3.3, Iset=0.8, vset=1.5(When pack voltage=3V) as expected according to the specification & requirement.
Additional details:
- STAT LED blinks when thermistor is removed as expected,
- LED is glowing constant, even when battery is not connected (tried to remove high value capacitors in the battery line, but still no results) which should be blinking as per the datasheet?
I've attached the schematic (Battery terminals are BAT & GND), please find the same.
We would really appreciate any help in solving this issue. Let me know if I can provide any additional information.
Thanks,