Hi,
There is no information about stability for constant on time regulators. Could you please tell me why there is no information about this ? I need fast response time but i need also that the output doesn't overshoot or undershoot too much ...
If i have a LC, i have a phase shift of 180 ° and with the negative feedback I have 180 ° and according to the stability criterion at 360° i should have a gain relatively low to prevent some oscillations ... I think i m missing something ... Why there is no problems of stability with this control mode ?
I did some measurements. I injected some pertubations on my feedBack, I measured the phase of the output and the phase of the feedback by changing the frequency of the pertubations, I did the same thing with the gain. ->>>> I Did a bode diagramm :D !
And the phase margin and gain margin are bad ... Below 42 ° for the phase margin which is bad :( I also made some step load because it is possible that i did bad measurements previously and i saw a lot of oscillation on my output voltage ... 0A5 to 3A - there is at least 2 oscillations ... I m looking for having only one overshoot or undershoot depending on the step load type ...
So if there is an explanation about why there is no problem of stability, i would be very happy :)
Maybe my ripple on the output voltage is too high or too low... Is this could explain my bad stability ? And if the stability depends on the ripple it would be nice to provide some informations about this :D Like this i could do compromises between stability and ripple :D
Thanks a lot ! :D and have a nice day !