Hi teams,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi teams,
Ninomiya-san,
I am not a UL expert, but I was able to find this link which discusses the topic of Coin Cell batteries in UL-certified applications on another site.
The resistor is used instead of adding a "fail-safe" diode in addition to the body diode of the CC to SYS_BU FET.
The article above links to another paper by a battery manufacturer that lists the maximum abnormal "charging" current that can be fed in to a reverse-biased coin cell battery. The most common value is 25mA.
The way to calculate the ideal current-limiting resistor depends heavily on the battery's internal series resistance.
I've made a few assumptions to calculate this number, but here is one way the 10-Ohms will work:
VSYS (input to IN_BU) = 4.2V (from the main Lithium Ion battery)
VCC (coin cell battery) = 3.0V (ideal voltage)
VFD (Diode drop across body diode from IN_BU to SYS_BU) = 0.6V
Diode from SYS_BU to CC has failed shorted.
RS (Internal series resistance of coin cell) = 15 Ohms
IREV,CC (reverse current into coin cell) = (VSYS-VFD-VCC)/(RS+10Ohms) = 0.024A < 25mA
This is just one example, and is only a 1st-order approximation. You can follow a similar procedure to get started determining the series resistance in your design.