I'm designing the active clamp flyback converter with UCC 28780. It seems that this controller works well in the CRM mode, but what if I want it to run in the continuous current mode (CCM)? I want to reduce the current ripple of the transformer, as a result, the magnetizing current is always positive. In this case, can the controller produce the PWM signal?
My second question is, I want to design the converter running at 1 MHz switching frequency, what components should I set up to design the switching frequency?
Thank you and looking forward to your response.