Hi guys,
I am asking a related question to something I posted a while ago. My customer designed two supplies with the TPS53319, where the initial component values were picked using webench and then modified as needed for an expected load current. One supply, 15V to 1V @ 9A is working well. The other supply, 15V to 3.3V @ 4A isn't. Now this supply was overdesigned and the load current ended up only being 1.5A. However, whenever there is a load step on the 3.3V supply (in the form of switching in a 47uF capacitor as a load) the transient response is slow and the input dips down to 2.8V
Can you guys take a look at the schematic and let me know if there is anything majorly wrong, and how you'd recommend we change it?
Thanks,
Brian