Part Number: LP5024
I have got LP5024 evm board.
I download LP50EVM GUI (Rev. A) from
http://www.ti.com/tool/LP5024EVM#technicaldocuments
But I still cannot control the evm board.
Addr0 and Addr1 all connect to ground with jumper.
So the i2c address is 0x28.
I also check vcc and vmcu both are 5V.
The connection status indicator at the bottom left corner is green.
But it still show can't read register.
Please help me check.