Hi,
What happens if the maximum load current is set to 7A, for example, and the adapter only provides 5A, for example? Will the BQ24610 work properly charging at 5A the battery or will it behave abnormally?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What happens if the maximum load current is set to 7A, for example, and the adapter only provides 5A, for example? Will the BQ24610 work properly charging at 5A the battery or will it behave abnormally?
Thank you.
Hi Ning T
I have a problem.
Charging current is lower than expected current.
ISET1 is 0.4V. that is, Maximum fast charge current is 2A.(But mearsured charging current is 1.3A)
ISET2 is 0.3V.
ACSET is 1.6V, Rac=0.2ohms. that is, Input Adapter current Regulation is 4A
depend on your reply, the reason is that DPM is working.
So, if it is right, How to modify without using DPM by ISET1,2,ACSET?