Other Parts Discussed in Thread: TPS3823, TPS3851, TPS3850
Hello,
I connected WDT to VDD and WDR to ground. The reset output is connected to the MCU Reset.
When I switch on the system, there is a reset every 3s after TPS3813 power up. However WDI stayed always low to be sure the watch dog is not running during MCU programming.
According to the datasheet :"After the first WDI low-to-high transition is detected, the lower boundary function of the window is enabled". So, if WDI is low, the watchdog should not start.
Am I right? If yes, why the watxchdog is starting?
Thanks for your support,
Damien