Hi,
Is it possible to use TPS2660 efuse to protect a 24V speaker? I have a potential use case as the following & will need advise if this would be the right device to perform this action.
Due to inbound power supply limitation on speaker, I'll need to drive the speaker at 1.1A only. If i were to lower the OCP settings to 1.1A, how will the efuse respond? And since audio is in sine wave >1kHz, will the output current clipped close to OCP values?
Regards,
Leo