We are currently working on a project involving BQ7791500pw, and saw an issue of load detection during OCD, OCC testing. It turns out that we forgot to place the resistor on the LD pin. Upon reading some documents, I realized that all the samples had the MOSFETs placed on the negative side. We had the MOSFETs placed on the positive side. Our question is this, for the load detection to work properly with MOSFETs on plus side, how do we place resistors at the 2 LD pins. Can we simply connect the top LD pin to the GND for top 4 cells, and connect a resistor of 470kOhm at the bottom stack from LD pin to B-? Thanks.