Part Number: TPS65132
I have this split-rail converter feeded with 3.3V, from a previous DC/DC converter (AAT1217ICA-3.3-T1). The TPS65132 It is loadad only with 1.6mA (resistive or linear) at both outputs. The whole system is feeded from an AAA battery. The layout is the same as recomended in the datasheet.
CASE 1: I turn on the system, and the TPS with all outputs disabled, and it's OK.
CASE 2: I turn on the system, and theTPS with outputs enabled and the inrush current is so high the previous converter cannot mantain the 3.3 and goes to a saturation state, the situation is permanent.
CASE 3: I turn on the TPS with the outputs disabled, and then enable POSitive, and after the NEGative, and sometimes, the error is the same.
The previous DC/DC is a AAT1217ICA-3.3-T1 (capable of an output current of 600mA)
The idea is to reduce this inrush current the TPS demands. The system works placing a high value capacitor (200uF), but not in the CASE 2. We want to avoid the use of this capacitor.
¿Can the TPS65132 operate with a 6.8uH or 10uH, or even more?
Thanks