Hi!
I am designing a power suplly with the UCC29950 controller, but i don´t known like i can make the inductor and transformer for the design. The power supply have a Vo=48V and 400W and the params with the document UCC29950 Design Calculator (Rev. A) are an inductor bigger than 402uH whit current peak 9.25A wiht f=100kHz. The transformer params are n=4, but i don´t know like i can choose the material and number turns for resonant circuit with a f=120kHz. There are some program for calculate the transformer and inductor characteristics.
thanks.