This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF3030: Need more information as references

Part Number: REF3030

Hi team,

Could you share below information? We are considering whether REF3030 can be used in the system. One big concern is the dropout voltage. In order to estimate the dropout voltage, we need these information. REF3033 has enough information, so we hope REF3030 has similar information with REF3330.

1. REF3330's Dropout Voltage vs Load Current for each temperature(I mean the figure in the datasheet P.1)

2. REF3030's more detailed Functional Block Diagram(I hope you can share it like REF3330).

3. REF3030's Dropout Voltage(max) at the temperature range from 0 to 70 degree C at I_load = 2mA.

Regards,

Noriyuki Takahashi