Hi,
I am building a 1.6kW CCM Boost PFC using UCC28180 Controller. Now I am gradually increasing the input voltage to power circuit from 0-230V and then turning on auxiliary supply to the controller. I am not using any pre-charge Diode in Boost circuit. If I put a precharge diode, Can I directly connect the circuit to a 230V socket and turn on everything at once? Will the UCC28180 controller will be able to stabilize the initial transient?