Hi Ti
We use TP51220A for dual dc dc output. Vout1 is 12V and Vout2 is 5V. Can we using the Vout2 connect to V5SW? The switch-over function is controlled by "Enable 1" , "PGOOD 1" and V5SW should be higher than 4.7V. Could you confirm any side effect when Vout2 connect to V5SW ? Can we only use the internal LDO without the switch over function?