This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BAttery charger IC with inputs from USB or Adaptor.



Hello All,

I want to use a BAttery Charger IC to charge a LIPO battery having a rating of 200mAH to 500mAH.

IC must be capable of showing status of battery voltages, includes all the protection as well must be able to charge battery in parallel providing voltage to the system also.

Input will be coming from Micro USB Connector.

Can you guys suggest, Which IC will be more praferable and upto what current ratings should i consider for charging 200-500 mAH LIPO battery.

Normal ratings of LIPO battery is 3V to 4.2V.

Please suggest me what should i keep in mind while selecting BAttery charging IC in terms of Voltage and current ratings of the IC.

Also share me any reference schematic to design the Hardware.  

Sharing a Block diagram of my hardware.