Other Parts Discussed in Thread: TPS2373-4EVM-758Hi Tom,
I'd be interested in a fully baked 90W 12V design. I found 24V/3A , 5V/14A, and 3.3V/30A designs but somehow haven't been able to find anything in the 12V range. I also see how both the 24V and 5V designs were built up on the same TPS2373-4EVM-758 board (with appropriate component changes). So it seems as if 12V would be pretty straight forward, especially if the output windings of T2 on PMP20758 were rewired in parallel. Do you have anything like that?