This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28631: Preload

Part Number: UCC28631


Hello,

I have the following design using a UCC28631. 

Vnom: 270V

Vout: Multiple

Po:80W.

The device needs a minimum preload value from Eqn 64 in datasheet, PPRELOADmin = 0.5 × LPRI× (VCS:min / RCS)^2 × fSW:min , but for my design to work I have to set my outputs preloads to almost 10W! 

My Lpri is 250uH (similar to the example equation) and my Rcs is 10 Ohms ( .2 Ohm going through 50:1 CT).