Hello,
The UCD9090 datasheet states that it is compliant with PMBus 1.1 specification.
Extract from the standard:
Extract from the datasheet:
Actually the 120ns is required for 1MHz PMBus clock - is this a typo or a real requirment?
Is the 120ns requirment in still place if the bus is used at 100kHz?
Is there a recommenced pull-up resistor to achieve 120ns TR for 400kHz?
Thank you