I am using UCD74120 to generate CVDD (1V) voltage for K2K SoC. On checking the voltage across the capacitor of value 220nF (as recommended in the datasheet) connected to BOOT pin of the same IC, it is expected that the output voltage across the same capacitor should be 1V, instead it is producing a voltage of 6V. This BOOT pin is connected to the SW pin of 74120 which is the output pin.
The schematic for the IC is same as that of the reference schematic.