This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2843: UC2843 Question about output stop of negative power supply.

Part Number: UC2843


Dear support member,

My customer made a negative power supply using UC2843.
When Iout 200mA, a phenomenon in which the output voltage stops has occurred.

I have a question.


Q1
Can IC work under this specification condition?

Specification condition
Vin:24V(±10%)
Vout:-15V~-24V
Iout:1A


Q2
Although the phenomenon that the output voltage stops has occurred,
Is it stopped by protection function?
Is there anything else cause?

Best regard.
Bob Lee.