Other Parts Discussed in Thread: LM3481
Hello Sir
I'm using LM3481MM/NOB converter IC in my project. It is chosen to operate at 550KHz. with a inductor with a value of 6.8 micro henry and with a input supply of 5V and to boost it up to 12V. While selecting the output capacitor only about current requirement is mentioned in the datasheet. No parameters or equations are mentioned in the datasheet to find the output capacitor value. So what is the minimum capacitance required for this design. Please help me out in this concern.
Regards
Nidhi P Shetty