Other Parts Discussed in Thread: TIDA-00779,
Team We are looking for a solution for a special power supply.
The power supply is operated either with 1 phase or 3 phases against the neutral.
With a 3-phase supply, I need an output line 4.5kW, with 1 phase is a reduced power
The output is 325V DC / No galvanic isolation
Is there a way to solve this with a reference design?


Input
Nominal Input Voltage 1x230VAC or as an option Nominal Input Voltage 3x230VAC
Line Frequency 40-70 Hz
Output
Nominal DC Output 325V DC
Max Output Power about 3000W @ 1x230VAC Input or as an option Max Output Power 4500W @ 3x230VAC Input
I can send you their drawing in direct message.
I hope it can be helped
Regards,
Naser