This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3808-Q1: Debounce time on RESET

Part Number: TPS3808-Q1


Team,

Does the TPS3808-Q1 have any debounce time associated with the falling edge triggering of a /RESET output pulse?

Thanks,

Fabio

  • Fabio,

    The debounce time associated with the input that causes a reset is defined as:

    Input pulse width to /RESET for SENSE pin: 20us typical
    Input pulse width to /RESET for /MR pin: 0.001us typical.

    Please see table 7.6 Switching Characteristics.

    Note: the debounce time is defined as minimum pulse width and is defined for the input pins that cause a /RESET.

    -Michael