Hi,
I'm designing Li-Ion battery charging station(adapter always ON) which will charge 2 series li-ion battery. The battery will be connected to be charged. The battery will be removed by the customer when charging is complete. By the way, the battery have a BMS for protection.
Chemistry/Cells: Li-Ion/2 series
Charging Voltage: 8.4V
Max. Charging Current: 1.4A
Adapter: ALWAYS ON
I have some questions for this design. Please give your comment.
1- I will not use system output. That's why I do not need any system output. I want to reduce external components of bq25703A because of board space and price. Please let me know, can I remove BATFET(P-Channel) ? I can use output capacitors for the BAT output.
I know that:
"If charge is disable, converter regulates the VSYS pin voltage about 160mV higher than VSRN. If without BATFET, the VSYS is almost short to VSRN, VSYS cannot meet VSRN+160mV set point. So, converter will keep pushing VSYS high until trigger OVP or other protection."
If there is any chance or suggestion for that, please let me know.