This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25601: The default charging setting of BQ25601 in host mode

Part Number: BQ25601

Hollo,

    I now use BQ25601 to set up a charging circuit ,but the charge current I need cannot exceed 1A,I read the specification that the default charging current is 2A,

    But there is a default power on the PESL control, when  PSEL is high power in host mode, the input current limit is 500mA,so does this limit start when the power is on or does it need to be enabled after the I2C     

    configuration,I charge I2C with 1A,will it have the default 2A charge when charged(I use a 5V adapter)