This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP Off Mode Using More Power than Retention

I am working on getting our system (OMAP3530 and TPS65950) to idle and sleep at its lowest power states possible.  I had assumed that enabling off mode (echo 1 > /debug/pm_debug/enable_off_mode) would lower the system power, but instead it goes up!  It is most obvious in suspend mode, where it uses 27mA more current from the TPS65950's 4.2V supply when enable_off_mode is 1 than when it is 0.

 

Note: Also posted to OMAP forum