Hello
Please help analysis my LEDs flicker problem,thanks
LED:10s/5p , SCH as attached(actually Rfb3 27Ω is renew to 27K, and Risense is 22mΩ,Rsense is 30mΩ not 20M);
Vin=12V ,VDD_5V and VDD3_3V is powered by external LDO, and its volatge is ok
SDO_PWM was pulled up to 3.3V ,all LP8863's resister is default not be changed, But LEDs is Flicker always.
Vboost about 30V has big ripple(maybe caused by LED current sink shut down)
GD signal and SW waveform plot as attached
SW_1 with 25KS/s sanning
SW_2 with 500MS/s scaning