Part Number: BQ76930
Other Parts Discussed in Thread: BQ76920
I would like to use the bq76930 to monitor a cell pack with a 10s1p configuration. The pack can enters (and also leave) in a special operation mode, the bq76930 switches to the SHIP Mode and after that the cell configuartion is changed. In this special mode the new arrangement of the 10s configuration is separated in two 5s configurations and connected parallel to each other. So that port VC10 is conneted with cell 10 and cell 5 and port VC5 (-b; -x) is connected with ground of cell 6 and ground of cell 1.Can the BMS chip be damaged by this re-configuration of the pack during the bq76930 is in SHIP mode?Tanks for your helpMarcel Bullen