Part Number: BQ33100
Hello,
I want to Write MAC command to BQ33100,
1. for Lifetime and Capacitor Balancing Enable (0x0021) the sequence will be:
Write Frame: Slave Address(0x16) => MAC (0x00) => SBS cmd (0x0021)
Write Frame: Slave Address(0x16) => MAC (0x00) => DATA 0x01 / 0x00
2. for rest of the MAC commands as there is no data part present, the sequence will be:
Write Frame: Slave Address(0x16) => MAC (0x00) => SBS cmd (0x0024)
--
as per my understanding; for part 2, we just need to write the command into MAC(0x00) and the action will take place in BQ33100; which is not the case for part 1 , there I have to perform separate i2c write transaction to load the action data into BQ33100
is this understanding correct?
Thanks.