Hello,
We are trying to configure one of the LGPO of the UCD9090-Q1 in state machine mode and so far we didn't achieve to reach our objectives.
Basically what we are trying to achieve is the following:
- At power-up, our LGPO is expected to be at low level.
- We expect the LGPO to change as when one of the GPI goes high.
- Once it has changed due to the GPI, we expect it to change when one of the monitoring input goes in a power-good off state (which basically means our input power is gone).
We tried different configurations of both the AND PATH 1 and AND PATH 2 without luck.
Could you help us point how we should be configuring both AND PATH ?
Perhaps one of the misunderstanding comes from the initial state of the LGPO. Is the AND PATH 1 used AND PATH 2 when we go out of reset ?
Thanks,
Clément