Other Parts Discussed in Thread: LM5117
Hi, can lm5141 work like lm5117 in continius current mode without hiccup(or re-softstart)?
Lm 5117 uses the RES pin : "The RES pin can also be configured for latch-off mode current limiting or non-hiccup mode cycle-by-cycle current limiting"
Does LM5141's RES pin have the same function?
And another question (lm4141) :
What will happen if in normal operation Vout increases (+10%) due to connection of an external power source (for example, a battery was connected) ? The Low Side mosfet will open and will stay open until the Vout is back to normal (or the mosfet is damaged ), or the bottom mosfet will stay open for one cycle, or something else?
Best Regards. Serj