Other Parts Discussed in Thread: UCC27533
Hi,
as below figure, when VDD is 7V, UCC27537 is till in off mode, but the IDD current is 300uA max current, what cause this high current?
in most case, UCC27537 is powered by auxiliary power, which has enough current capacity.
but now, one customer use UCC27537 in flyback auxiliary power supply, to drive flyback primary low side IGBT.
at startup, the flyback IC and driver UCC27537 is powered by pre-charge resistor, the pre-charge current is small, IDDoff current will make flyback IC has no enough VDD voltage to turn on.
question:
1. what cause this high current inside UCC27537?
2. this test is at VDD 7V, if VDD voltage is 3V or lower, is this current smaller?
3. are there some methods to solve this problem?