Part Number: BQ76940EVM
Other Parts Discussed in Thread: BQ78350-R1, BQ76940
Hello,
I'm currently working with the BQ76940EVM, EV2300 and the latest BqStudio version (1.3.86.3). I already used the GPC packer to get better SoC values. The BQ76940EVM worked quite good a while ago but somehow it turned bad without making any changes. I programmed the default firmware again and adjusted the settings again, but the SoC estimation is still wrong. It happens that the value of the SoC jumps to 0% or 100 % without making sense in the middle of a test. I have no idea why or what I can change. I attach a log file including some manual resets and test interruptions to get the correct SoC again and the actual gg file. I also attach the results of the GPC packer. I'm happy about any held.
regards Anna