Part Number: LM3434SQ-20AEV
Hi
I tasked to design LEDs panel dimmer for up to 15A with 17V Leds strips i found the LM3434 best fit for the task and the LM3434SQ-20AEV for first evaluate.
I bought 2 units of LM3434SQ-20AEV from TI store for evaluating LEDs dimmers for LED lights panel.
I connect the evm to lab DC power supply with maximum 3A output current and to 4 x 17V ( 6 leds of 2.7V 600ma) LEDs strips and 15khz PWM connected to between GND and PWM input.
The First board EVM the dimming not function there was no response to duty cycle change of PWM and after one minute the board stop driving the LEDs and start to consume hi current (shortcut ),Q4 and Q3 temperature rise to more then 60C.
The second EVM function as expected. Except for when setting the PWM duty to get 100% power and the increase the PWM to reduce the output it stuck in 100% till power down and up again.
After running the second EVM for 20 minutes it stop driving the LEDS and the output voltage on the LEDs remain 16V and nothing help .
Please advice ?
Thanks
Ofer Merom