Other Parts Discussed in Thread: TPS7A91, TPS7A91EVM-831
Hello LDO TEAM
When I use LDO TPS7A92 ,input voltage 5V and output voltage is 3.3V.
The input capcitor is one 10uF/25V MLCC in parallel with one 220uF/16V AL CAP.
While output capcitor is one 10u/25V MLCC CAP in parallel with one 220uF/16V AL CAP.and the load current is about 500mA.
Please help to make sure that the input and output capcitor meet the requirements of circuit stability
Very Respectfully
Cheney_Sun