Part Number: TPS1663
Other Parts Discussed in Thread: TPS2660, LM5060
Customer is interested in the TPS16630 with HTSSOP package. Is this RTM already? if not so, when?
Regards,
brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Regarding to the OVP fuction with the TPS16630, how is that failure mode during OVP event? Latch or Auto-Retry?Or it can be programmable for either one?
One more, except the TPS16630 with 6A,max current, customer is very interested in it but the price is NOT able to meet their target of bom cost. Is there other device similar to TPS16630 with lower current rating of 2A or 3A? The real current in application is just 1.5A. Very thanks.
Application: Safety function on VFD control board.
Potential Volume: 1.5-2Mu/year
Target price: 0.xx
Regards,
Brian