Hi, I'm using the BQ25890H in a system with a replaceable battery. I observe that Vsys seems to have a slow, high magnitude ripple when the charger is powered from USB, but the battery is disconnected. I'm just starting to dig into it, but right now it seems like the NVDC charger is hunting from the minimium VSYS up to 4.2 + the dropout over a 10s of ms period. Is this known/typical? Are there settings I can modify in the BQ25890H to reduce/eliminate this? Is operating the BQ25890H without a battery a supported mode of operation?
Thanks!