This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54335A: Schematic validation

Part Number: TPS54335A


Hello,

I am finalizing my design of a BUCK supply based on TPS54335A, and I would like that some TI engineer validate my schematic, please.

Vin = 23.5 to 28V 

Iout = 507 mA / 1.7 A peak

T° range : 5°C to 70°C

Regards,