Hi,
The major customer is considering to use bq25898 and they plan to use following fast charge current setting. Then they 'd like to know the estimated accuracy at these setting. I know that you can guarantee +/- 5% at 1792mA setting, so I guess that the accuracy will be decreased at these setting. so please let me know the estimated min/max accuracy at these setting? I understand that you can't guarantee it so rough information should be enough as just for information.
- 1088mA
- 1152mA
- 1216mA
Best Regards,
Satoshi