I am planning to design a Li Ion battery charge circuit using IC BQ24650.
I need to take power from the battery while charging it with out disturbing the charging parameters.Is it possible?
Can I take system power from "up side" of the current sense resistor-(SRP pin.) From which point of the application circuit , I can connect the load?
And also in all the application notes of Li-Ion charging, lower value current of constant current phase is not mentioned. Can you please suggest a minimum current setting in constant current phase.
thank u.