Hello,
I am trying to complete a learning cycle for my single Samsung1.5 Ah NMC power cell with a BQ40z50 EVM board. After a few initial hiccups, I was able to work through all of the steps outlined in this learning cycle guide and everything was going as expected up until the post C/5 discharge rest period when Update Status never went to 06. It has been stuck at 05 since the post charge rest period. Interestingly, QMAX and the Resistance Table for the cell have updated, and my Cell0 R_a Flag is now set to 5555. I believe these three things indicate that the learning cycle was successful, but I’m not sure because Update Status is not 06, as the learning cycle document says it should be.
My question is this: Why is my Update Status not going to 06? Does this indicate that my learning cycle was not successful, even though QMAX and Resistance tables are updating?
An outline of the steps I am taking from start to finish can be found here.
A register log file for the learning cycle can be found here. The discharge data being around 13:00 on 10/10/2018. The associated error log can be found here.
A data memory gg.csv file from right before the C/5 discharge was started (end of post charge rest period) can be found here.
A data memory gg.csv file from midway through the C/5 discharge can be found here.
A data memory gg.csv file from immediately after the C/5 discharge completed can be found here.
A data memory gg.csv file from 12+ hours into the C/5 discharge rest period can be found here.
Please let me know if you have any specific questions, or if more data would be helpful, as I have many more gg.csv files I could share.
Thank you,
-Zander