UCD3138 has an example implementation PFC
Curious question: if the line current is forced to be in phase with the line voltage, then the "converter" is presenting a " positive resistive " load to the ac system "on the average"..
Yet, the converter is a " constant power load (CPL)- which is characterized by a "negative" input impedance.
How do we reconcile these two?
Is it possible to instrument for measuring the input impedance of such a converter by code in the UCD? The display is of course the computer is it connected to via the PMBus.
Then why not the loop response as well by code? Because all sensors are there in the circuit.
thnx
robin