I would like to know if this can be used in this way. typical application QOD is connected to VOUT via R for discharge. but what I am thinking is enabling for DC/DC, QOD is for output of DC/DC which needs quick discharging. regards, NY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like to know if this can be used in this way. typical application QOD is connected to VOUT via R for discharge. but what I am thinking is enabling for DC/DC, QOD is for output of DC/DC which needs quick discharging. regards, NY
Hi NY,
Thanks for reaching out on E2E.
I see a potential issue with VOUT of the TPS22810. There's nothing to pull-down the output of the load switch, so it might remain floating if EN is disabled. Could you simply put the TPS22810 at the output of the DC/DC converter, and use the QOD in that way?
Thanks,
Arthur Huang