Hi,
I have some question about the control method in UCC28780.
1. In AAM, it is peak current mode control. The peak current of sense resistor is determined by the Ifb to regulate the output voltage.
How does Ifb generate the reference of the peak current in AAM mode?
2. In ABM, the ripple waveform of Ifb determines the burst-on point when Ifb intersect the IREF.
What is the IREF in figure 41? How does it generate?
3. In LPM,the peak current of sense resistor is determined by Ifb to regulate the output voltage.
How does Ifb generate the reference of the peak current in LPM mode?
4. In SBP mode, the burst frequency is determined by Ifb to regulate the output voltage.
How does Ifb generate the reference of burst frequency in SBP mode?
BR
Eleven Chen