This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92641: About “PWM Dimming Using the UDIM Pin” and “External Shunt FET PWM Dimming”

Guru 21045 points
Part Number: TPS92641

Hi Team,

 

I would like to know use “PWM frequency is around 120Hz” and “Duty is 20% to 40%”.

So, I have two questions.

 

[Q1]

Can I input “PWM frequency is around 120Hz” and “Duty is 20% to 40% to UDIM pin

 

[Q2]

Can I input “PWM frequency is around 120Hz” and “Duty is 20% to 40% to SDIM pin

 

Regards,

Kanemaru