This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9246: i2c/PMBus programming

Part Number: UCD9246
Other Parts Discussed in Thread: UCD9090,

Dear Yihe,

We understood more and more how the device works.
Unfortunately, we need to do that not reading a documentation, but wasting your and our time in the dialog.
In our case we can't really follow the script you sent to us.
The problem is that we don't have the information from the 1k sector program flash which we need to erase (the customer gives us the file with data flash only).
So as we understand, we need to read the 1k program flash before erasing.
Summary our questions are:
- should i read the 1k program flash before erasing? If i need that, please, send the particular commands (script example) how to do that (there is no information anywhere).
- should i program all read locations back OR we should mask (write 0xFF) the Program Flash Integrity Word? If yes, what is the Program Flash Integrity Word location?
- should i use the command Verify Checksum ROM (Integrity Word) according to the script? Really i can't verify this value, because, firstly, i don't have the Program Flash content, secondly, i don't know the algorithm of checksum calculation.
- i noticed that script uses absolute address but not offset as UCD9090 does. Does it mean i should use absolute address then i will read data flash?
- script uses command 0xfd (device_id) among other commands. Does it mean that command can vary its meaning depending of the mode?

- is there a mechanism (script) to recover device from ROM_MODE in order i can recover a device apart from Fusion tool? if yes, can you send it to me as well?

I will be very appreciated if you answer on all my questions.
And I will be out of office all next week and will continue to the work after that.

Thank you

  • dmitry ivanov said:

    Part Number: UCD9246

    Dear Yihe,

    We understood more and more how the device works.
    Unfortunately, we need to do that not reading a documentation, but wasting your and our time in the dialog.
    In our case we can't really follow the script you sent to us.
    The problem is that we don't have the information from the 1k sector program flash which we need to erase (the customer gives us the file with data flash only).
    So as we understand, we need to read the 1k program flash before erasing.
    Summary our questions are:
    - should i read the 1k program flash before erasing? If i need that, please, send the particular commands (script example) how to do that (there is no information anywhere).

    [TI] The 1K flash is fixed and it is already inside the script file. you do not have to read again, you just need follow that file.
    - should i program all read locations back OR we should mask (write 0xFF) the Program Flash Integrity Word? If yes, what is the Program Flash Integrity Word location?
    - should i use the command Verify Checksum ROM (Integrity Word) according to the script? Really i can't verify this value, because, firstly, i don't have the Program Flash content, secondly, i don't know the algorithm of checksum calculation.

    [TI]if you look at the end of script, it call 0xEF to calcuate the checksum and 0xEE to read the checksum. the script has done everything for you. The checksum is located 0x7FFC

    - i noticed that script uses absolute address but not offset as UCD9090 does. Does it mean i should use absolute address then i will read data flash?

    [TI] follow what the scrips tell you to do. UCD9090 does not required ROM mode to program but UCD9246 does. so there are differences.
    - script uses command 0xfd (device_id) among other commands. Does it mean that command can vary its meaning depending of the mode?

    [TI]Yes, you are right. 0xFD has different meaning which is up to device's mode(PROGRAM MODE and ROM MODE).

    - is there a mechanism (script) to recover device from ROM_MODE in order i can recover a device apart from Fusion tool? if yes, can you send it to me as well?

    [TI] currently, we do not have such tool other than fusion GUI.

    I will be very appreciated if you answer on all my questions.
    And I will be out of office all next week and will continue to the work after that.

    Thank you

  • Dear Yihe,

    We are working now with UCD9246. If you remember we have entered to the ROM Mode and could not recover it back.
    We have got USB-TO-GPIO and was able to recover the device.
    After that I tried to _strictly_ follow to the script you sent to me.
    My problems:
    1. I always needed to use PEC during programming. Otherwise I received NACK.
    You noticed that PEC is optional. Can you explain why we were really needed to use PEC?

    2. As I have already wrote we strictly followed the script.
    It consists of the following steps:
    a) Sending device to ROM mode....passed without errors
    b) Mass erasing data flash.....passed without errors
    c) Write data flash...passed without errors
    d) Erasing last segment of program flash ......passed without errors
    e) Write program flash with data from the script...passed without errors
    f) Having ROM calculate the program flash checksum...passed without errors
    g) Verifying checksum ROM calculated matches what we wrote.....!!!!
    On this step we get data from the device which was different from the script data.
    Probably it means that checksum is wrong, doesn't it?
    h)Executing program...passed without errors

    After the last step device became "brick" and does not reply absolutely.
    My questions:
    2.1 Why do we get the checksum from the device not equal script checksum?
    2.2 How can we recover the device from this state?

    3. In the installed software for USB-TO-GPIO we have discovered the utility "Fusion Tool Launcher" (in the folder ...\Texas Instruments\Fusion Digital Power Designer\bin)
    which is likely can be useful to recover the brick device.
    But it asks the program Flash hex file for recovering. Can you send us this file?

    Please, answer on _all_ our questions.
  • 1. When device is under ROM mode, PEC byte is mandotary, it is only optional when device is under normal mode.

    2. Does your device have the correct device ID: UCD9246-64|5.6.0.11220|090922 as described in the script file? If not, your can not use the script file i shared.

    From the script file, you would write 0x66DBEBB2EEEBBBB833B5EE00002C55D6C7 to address 0x17FF0, where 2C55D6 is the checksum. on the step g, the returned checksum shall be 2C55D6. if it is not, the device will stay at the ROM mode and you need to flash a factory data to solve this.

    3. Below is the file, you can use the Fusion Firmware and configuraiton download tool to un-brick the device.https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/UCD9246_2D00_64_5F00_5.6.0.11220.x0

    Regards

    Yihe

  • Yihe

    You wrote we must have device with ID: UCD9246-64|5.6.0.11220|090922 otherwise we cannot use your script. 

    It means that we can program ONLY devices with this ID. But the reasonable question is what we should do with other IDs, they could not be programmed? (f.e. i have ID: UCD9246-64|5.7.0.11359|091029)
    Is there universal approach to program the device?
    We see to ways:
    - read the program-flash and write it back, but we don't have information how the reading works. Does the device have such opportunity to read flash back?
    - always write particular firmware in all devices. But I believe it's not a good way, because the device can have a newer one.


    What about  the  Fusion-tool, how does it work to cover all versions of frameworks?

    Regards

  • I hope that you understand that the script file is not compabilible cross different device. The approach is the same but you can not mix the script with device
    If you look the script file i provided, the first step it is to read the DEVICE_ID, you have to make sure the DEVICE_ID from the device matches the script file. The script file I provded is only for UCD9246-64|5.6.0.11220|090922.

    For any device you are working on, you need export the script file yourselves.

    Regards

    Yihe
  • Dear Yihe,

    Nice that you thought that we are so smart understanding that this script is only for one ID. We are not so smart without any information from you.
    Nevertheless, we need to support ALL ID versions on the customer end.
    We see that TI tool can create the script file for different IDs. So you have a way to do that.
    It seems that we need this technology.
    If we need to sign any additional NDA to get this technology, let me know the person with whom we can resolve this question.
    If we don't need to resolve some organizational questions, please clarify how we can create script file ourself.

  • For each ID on your customer end, your customer will provide a separated script file to program.
    What you need is to follow the script and write the data into the device which have the same ID as your script file.
    I do not see why you need the capability of the GUI. the script file must be from fusion GUI.
    Regards
    Yihe
  • Dear  Yihe,

    As we have said you that our current customer now is Flextronix (a very big manufacturing company).
    They provides us with file contains only the EEPROM data.
    I am absolutely sure that they don't know what the script is and how they can generate it.
    Moreover they produce a lot of equipment and may be the situation when there are devices with different IDs in one manufacturing batch.
    In this situation (according to your rules) when they meet a device with a new ID (we can't support it, because don't have according script),
    they have to stop manufacturing, send us a board (we can't generate a script without a particular device with a new ID and connecting it to TI tool), waiting for the board delivery to our lab (it may be a few weeks, and they are waiting at this time)  and etc.
    Do you mean that we need to follow to this rule?
    If yes, in our experience, it's the really most original way to support customers, we have never met anything similar.
    We will send you suggestions to Flextronix and will send you their feedback.

  • Hello
    Thank you for bringing this. Recently, TI have releaesd a series UCD90xxx training video. The following one is to train customer how to generate data flash script file
    training.ti.com/fusion-power-designer-how-import-and-export-data-flash-script-files.

    When a new ID prodcut is released by TI, Fusion GUI is capable to generate the script file. Your customer will always need TI Fusion GUI to configure the device regardless. Without fusion GUI, they can not configure/tune the device. once they have all the design fixed, they will export the data flash script file and provide the file to you. what you need is to follow the file and program into the device.
    Hope this clear your concerns.

    Regards
    Yihe
  • Hi Dmitry,

    As we don't hear from you for weeks, we are closing this post. Please let us know if you have more questions.

    Thanks
    Qian