Other Parts Discussed in Thread: TPS56628, TPS568215, TPS54628
Hello!
I am wondering if it is OK that TPS54821 EVB draws 14mA without load with 12V input voltage?
My design with 5V output draws about 24mA.
My design requirments are:
- Up to 5A 5V output
- 8-13V input
- Small idle current
- Small footprint
- Little thermal emissions
- Low cost of course :)
Could someone advice if I can do something to decrease idle power consumption or recommend better part for my design?
Kristaps